public interface TCP
Modifier and Type | Method and Description |
---|---|
String |
getDisplayName()
Note: The TCP can be renamed at any time
|
Pose |
getOffset() |
boolean |
isResolvable() |
Pose getOffset()
String getDisplayName()
boolean isResolvable()
true
, if the TCP is present in PolyScope. true
, if the TCP is not present (e.g. a different
installation is used, the TCP has been removed by the end user or the URCap adding it, at some point in time, has
removed it).Copyright © 2019. All rights reserved.