public interface GripVacuumCapability
This interface represents a registered vacuum capability for a gripper which supports gripping using a user configurable vacuum level.
Through this interface, it is possible to adjust the range and default value for the vacuum level after the capability has been registered. This is typically not applicable for most grippers, but can be relevant when the range depends on another custom gripper setting (which can be configured by the user).Modifier and Type | Method and Description |
---|---|
void |
updateCapability(double minVacuum,
double maxVacuum,
double defaultGripVacuum,
Pressure.Unit unit)
Update the range and default value for the vacuum level supported by the gripper.
|
void updateCapability(double minVacuum, double maxVacuum, double defaultGripVacuum, Pressure.Unit unit)
Update the range and default value for the vacuum level supported by the gripper.
Updating the range could result in an already entered value in the configuration of a gripper program node being outside the range. This will make the given program node undefined, and force the end user to adjust the value to be valid again.
If the gripper works with absolute pressure, specify a positive range for the supported vacuum level. If the gripper works with relative pressure (vacuum), specify a negative range for the supported vacuum level.minVacuum
- minimum vacuum level supported by the grippermaxVacuum
- maximum vacuum level supported by the gripperdefaultGripVacuum
- default value for the vacuum level for a grip action. This value is used for, e.g.
performing a "default" grip action using the toolbarunit
- the unit for all specified values, not null
InvalidCapabilityRange
- if minVacuum
> maxVacuum
or defaultGripVacuum
is outside the
range defined by minVacuum
and maxVacuum
.Copyright © 2019. All rights reserved.