public interface SimpleValueFactory
| Modifier and Type | Method and Description | 
|---|---|
Acceleration | 
createAcceleration(double value,
                  Acceleration.Unit unit)
Creates an object representing an acceleration value 
 | 
Angle | 
createAngle(double value,
           Angle.Unit unit)
Creates an object representing an angle value 
 | 
AngularAcceleration | 
createAngularAcceleration(double value,
                         AngularAcceleration.Unit unit)
Creates an object representing an angular acceleration value 
 | 
AngularSpeed | 
createAngularSpeed(double value,
                  AngularSpeed.Unit unit)
Creates an object representing an angular speed value 
 | 
Current | 
createCurrent(double value,
             Current.Unit unit)
Creates an object representing an electrical current value 
 | 
Force | 
createForce(double value,
           Force.Unit unit)
Creates an object representing a force value 
 | 
Length | 
createLength(double value,
            Length.Unit unit)
Creates an object representing a length value 
 | 
Pressure | 
createPressure(double value,
              Pressure.Unit unit)
Creates an object representing a pressure value 
 | 
Speed | 
createSpeed(double value,
           Speed.Unit unit)
Creates an object representing a speed value 
 | 
Time | 
createTime(double value,
          Time.Unit unit)
Creates an object representing a time value 
 | 
Torque | 
createTorque(double value,
            Torque.Unit unit)
Creates an object representing a torque value 
 | 
Voltage | 
createVoltage(double value,
             Voltage.Unit unit)
Creates an object representing an electrical voltage value 
 | 
Length createLength(double value, Length.Unit unit)
value - length value in specified unitsunit - type of unit for the value argumentLength objectSpeed createSpeed(double value, Speed.Unit unit)
value - speed value in specified unitsunit - type of unit for the value argumentSpeed objectAcceleration createAcceleration(double value, Acceleration.Unit unit)
value - acceleration value in specified unitsunit - type of unit for the value argumentAcceleration objectAngle createAngle(double value, Angle.Unit unit)
value - angle value in specified unitsunit - type of unit for the value argumentAngle objectAngularSpeed createAngularSpeed(double value, AngularSpeed.Unit unit)
value - angular speed value in specified unitsunit - type of unit for the value argumentAngularSpeed objectAngularAcceleration createAngularAcceleration(double value, AngularAcceleration.Unit unit)
value - angular acceleration value in specified unitsunit - type of unit for the value argumentAngularAcceleration objectForce createForce(double value, Force.Unit unit)
value - force value in specified unitsunit - type of unit for the value argumentForce objectTorque createTorque(double value, Torque.Unit unit)
value - torque value in specified unitsunit - type of unit for the value argumentTorque objectCurrent createCurrent(double value, Current.Unit unit)
value - electrical current value in specified unitsunit - type of unit for the value argumentCurrent objectVoltage createVoltage(double value, Voltage.Unit unit)
value - electrical voltage  value in specified unitsunit - type of unit for the value argumentVoltage objectTime createTime(double value, Time.Unit unit)
value - time value in specified unitsunit - type of unit for the value argumentTime objectPressure createPressure(double value, Pressure.Unit unit)
value - pressure value in specified unitsunit - type of unit for the value argumentPressure objectCopyright © 2019. All rights reserved.