public static enum Voltage.Unit extends Enum<Voltage.Unit>
Enum Constant and Description |
---|
V
Volt [V] SI unit
|
Modifier and Type | Method and Description |
---|---|
static Voltage.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Voltage.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Voltage.Unit V
public static Voltage.Unit[] values()
for (Voltage.Unit c : Voltage.Unit.values()) System.out.println(c);
public static Voltage.Unit valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.