public static enum Length.Unit extends Enum<Length.Unit>
| Enum Constant and Description | 
|---|
IN
Inches [in] imperial unit 
 | 
M
Meters [m] SI unit 
 | 
MM
Millimeters [mm] 
 | 
| Modifier and Type | Method and Description | 
|---|---|
static Length.Unit | 
valueOf(String name)
Returns the enum constant of this type with the specified name. 
 | 
static Length.Unit[] | 
values()
Returns an array containing the constants of this enum type, in
the order they are declared. 
 | 
public static final Length.Unit M
public static final Length.Unit MM
public static final Length.Unit IN
public static Length.Unit[] values()
for (Length.Unit c : Length.Unit.values()) System.out.println(c);
public static Length.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2019. All rights reserved.