| Interface | Description | 
|---|---|
| Capability | 
 
 This marker interface represents a capability that may or may not be available on the underlying robot/system. 
 | 
| CapabilityManager | 
 
 This interface can be used to query whether or not a specific capability is available on the underlying robot/system. 
 | 
| Exception | Description | 
|---|---|
| CapabilityNotSupportedException | 
 This exception is thrown when trying to use a capability which is not supported by the underlying robot/system. 
 | 
Copyright © 2019. All rights reserved.