@RequiredCapability(value=DIGITAL_OUTPUT_MODE) public interface DigitalOutputModeConfigFactory
Factory for creating configurations of the digital output mode for the digital outputs in the connector in the robot tool.
UseCapabilityManager.hasCapability(Capability) with ToolIOCapability.DIGITAL_OUTPUT_MODE
 to verify the availability of this functionality on the system.| Modifier and Type | Method and Description | 
|---|---|
DigitalOutputModeConfig | 
createDualPinPowerModeConfig()
Create a Dual Pin Power mode configuration where both digital outputs in the connector in the robot tool are used
 as a source of power for the tool. 
 | 
StandardDigitalOutputModeConfig | 
createStandardDigitalOutputModeConfig(StandardDigitalOutputModeConfig.OutputMode output0,
                                     StandardDigitalOutputModeConfig.OutputMode output1)
Create a configuration to set the digital output mode for each of the digital outputs in the connector in the
 robot tool. 
 | 
DigitalOutputModeConfig createDualPinPowerModeConfig()
StandardDigitalOutputModeConfig createStandardDigitalOutputModeConfig(StandardDigitalOutputModeConfig.OutputMode output0, StandardDigitalOutputModeConfig.OutputMode output1)
output0 - the output mode for digital tool output 0output1 - the output mode for digital tool output 1Copyright © 2019. All rights reserved.