public interface PoseFactory
| Modifier and Type | Method and Description |
|---|---|
Pose |
createPose(double x,
double y,
double z,
double rx,
double ry,
double rz,
Length.Unit lengthUnit,
Angle.Unit angleUnit)
Creates a
Pose object with the specified Cartesian position and orientation (rotation) |
Pose createPose(double x, double y, double z, double rx, double ry, double rz, Length.Unit lengthUnit, Angle.Unit angleUnit)
Pose object with the specified Cartesian position and orientation (rotation)x - x-coordinate of the positiony - y-coordinate of the positionz - z-coordinate of the positionrx - rx-parameter of the rotation vector specifying the orientationry - ry-parameter of the rotation vector specifying the orientationrz - rz-parameter of the rotation vector specifying the orientationlengthUnit - enum to specify the position unit typeangleUnit - enum to specify the rotation unit typeCopyright © 2018. All rights reserved.