public static enum Length.Unit extends Enum<Length.Unit>
| Enum Constant and Description |
|---|
IN
Inches [in] imperial unit
|
M
Meters [m] SI unit
|
MM
Millimeters [mm]
|
| Modifier and Type | Method and Description |
|---|---|
static Length.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Length.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Length.Unit M
public static final Length.Unit MM
public static final Length.Unit IN
public static Length.Unit[] values()
for (Length.Unit c : Length.Unit.values()) System.out.println(c);
public static Length.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2018. All rights reserved.