public static enum Torque.Unit extends Enum<Torque.Unit>
| Enum Constant and Description |
|---|
LBFT
Pound-foot [lb·ft] imperial unit
|
NM
Newton meters [N⋅m] SI unit
|
| Modifier and Type | Method and Description |
|---|---|
static Torque.Unit |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static Torque.Unit[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final Torque.Unit NM
public static final Torque.Unit LBFT
public static Torque.Unit[] values()
for (Torque.Unit c : Torque.Unit.values()) System.out.println(c);
public static Torque.Unit valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2018. All rights reserved.