public interface FunctionModel
InstallationNodeContribution.generateScript()
The full set of functions which can be contributed must be added in the preamble at all times,
regardless of whether they are added to the Expression Editor or not.
Otherwise old programs that rely on a script function contribution might stop working.Function| Modifier and Type | Method and Description |
|---|---|
Function |
addFunction(String name,
String... argumentNames) |
Function |
getFunction(String name) |
Collection<Function> |
getFunctions(Filter<Function> filter) |
boolean |
removeFunction(Function function) |
Function addFunction(String name, String... argumentNames) throws FunctionException
name - Name of the function. Safe names must match regex [a-zA-Z][a-zA-Z0-9_]{0,24} for a total of 25 characters. A range of Universal Robots reserved names
exists and cannot be used. In case of an illegal or reserved name, an FunctionException will be thrown.argumentNames - Is a list of hints (for the function arguments) to be shown comma separated inside angle brackets in the Expression Editor.
No more than five arguments can be specified. The hints must also match the regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a total of 15 characters.
Otherwise an FunctionException will be thrown.FunctionException - if the name is illegal or more than five arguments are specified.boolean removeFunction(Function function)
function - Function to be removed. Only functions added by this URCap can be removed.Function getFunction(String name)
name - The name of the function.Collection<Function> getFunctions(Filter<Function> filter)
filter - The filter being applied to the full list of added functions (by URCaps).Copyright © 2018. All rights reserved.