public static enum CreationContext.NodeCreationType extends Enum<CreationContext.NodeCreationType>
| Enum Constant and Description |
|---|
LOAD
This node was created as the result of loading an installation
|
NEW
This node was created as the result of creating a new installation
|
| Modifier and Type | Method and Description |
|---|---|
static CreationContext.NodeCreationType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CreationContext.NodeCreationType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CreationContext.NodeCreationType NEW
public static final CreationContext.NodeCreationType LOAD
public static CreationContext.NodeCreationType[] values()
for (CreationContext.NodeCreationType c : CreationContext.NodeCreationType.values()) System.out.println(c);
public static CreationContext.NodeCreationType valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2018. All rights reserved.