| Class and Description |
|---|
| VariableModel
Provides methods that returns the variables that currently are registered in the system.
|
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| Variable |
| Class and Description |
|---|
| FeatureVariable
A Feature marked as a Variable in the installation will exist even when a robot is turned off and on.
|
| GlobalVariable
Global variables are available everywhere in a program.
|
| PersistedVariable
This interface represents variables stored with the installation.
|
| Variable |
| Variable.Type
The variable type used to determine which type of variable this instance is.
|
| VariableException
This exception is thrown if a Variable has an illegal name.
|
| VariableFactory
This interface supplies methods to create variable objects.
|
Copyright © 2021. All rights reserved.