| Interface | Description |
|---|---|
| Payload |
This interface represents a payload from the installation in PolyScope.
|
| PayloadContributionModel |
This interface provides functionality for adding, updating and removing payloads in PolyScope.
|
| PayloadModel |
This interface provides access to the payloads that are currently available in the installation in PolyScope.
|
| Enum | Description |
|---|---|
| Payload.ParametersWarning |
This enum represents the different types of warnings that the parameters of a payload can have.
|
| Exception | Description |
|---|---|
| IllegalCenterOfGravityException |
This exception is thrown if any of the values of the specified center of gravity are outside the valid range, as
defined by PolyScope, when an attempt is made to add or update a payload (using the
PayloadContributionModel
interface). |
| IllegalInertiaMatrixException |
This exception is thrown if any of the values of the specified inertia matrix are outside the valid range, as
defined by PolyScope, when an attempt is made to add or update a payload (using the
PayloadContributionModel
interface). |
| IllegalMassException |
This exception is thrown if the specified payload mass is outside the valid range, as defined by PolyScope, when an
attempt is made to add or update a payload (using the
PayloadContributionModel interface). |
| IllegalPayloadNameException |
This exception is thrown to indicate that a payload with an illegal suggested name has been requested to be added to
the installation in PolyScope (using the
PayloadContributionModel interface). |
| PayloadAlreadyAddedException |
This exception is thrown if a payload has been requested to be added to the installation in PolyScope (using the
PayloadContributionModel interface) when the payload is already present. |
| PayloadNotFoundException |
This exception is thrown when attempting to modify or remove a payload (using the
PayloadContributionModel
interface) that does not exist in PolyScope. |
Copyright © 2021. All rights reserved.