| Package | Description |
|---|---|
| com.ur.urcap.api.contribution.driver.gripper |
| Modifier and Type | Method and Description |
|---|---|
void |
GripperContribution.configureGripper(GripperConfiguration gripperConfiguration,
GripperAPIProvider apiProvider)
When this method is called, use the configuration parameter to register or setup optional properties and capabilities
of the gripper.
|
void |
GripperContribution.configureInstallation(CustomUserInputConfiguration customConfiguration,
SystemConfiguration systemConfiguration,
TCPConfiguration tcpConfiguration,
GripperAPIProvider apiProvider)
When this method is called, required configuration related to the setup of the gripper can be defined/performed,
e.g.
|
Copyright © 2021. All rights reserved.