@RequiredCapability(value=DIGITAL_OUTPUT_MODE) public interface DigitalOutputModeConfigFactory
Factory for creating configurations of the digital output mode for the digital outputs in the connector in the robot tool.
UseCapabilityManager.hasCapability(Capability) with ToolIOCapability.DIGITAL_OUTPUT_MODE
to verify the availability of this functionality on the system.| Modifier and Type | Method and Description |
|---|---|
DigitalOutputModeConfig |
createDualPinPowerModeConfig()
Create a Dual Pin Power mode configuration where both digital outputs in the connector in the robot tool are used
as a source of power for the tool.
|
StandardDigitalOutputModeConfig |
createStandardDigitalOutputModeConfig(StandardDigitalOutputModeConfig.OutputMode output0,
StandardDigitalOutputModeConfig.OutputMode output1)
Create a configuration to set the digital output mode for each of the digital outputs in the connector in the
robot tool.
|
DigitalOutputModeConfig createDualPinPowerModeConfig()
StandardDigitalOutputModeConfig createStandardDigitalOutputModeConfig(StandardDigitalOutputModeConfig.OutputMode output0, StandardDigitalOutputModeConfig.OutputMode output1)
output0 - the output mode for digital tool output 0output1 - the output mode for digital tool output 1Copyright © 2020. All rights reserved.