@ProviderType
public interface SelectableGripper
MultiGripperSupport interface). The gripper is selectable by the end user
when configuring a Gripper program node for a multi-gripper device.| Modifier and Type | Method and Description |
|---|---|
String |
getDisplayName()
The name of the gripper displayed in the PolyScope UI, e.g.
|
String |
getId()
Get the unique identifier (id) for this gripper.
|
boolean |
isResolvable()
An individual gripper cannot be guaranteed to be present in PolyScope.
|
String getId()
Get the unique identifier (id) for this gripper. This can be used to identify this specific gripper among the set of individual grippers available in a specific multi-gripper device.
Note that this id is not "globally" unique, but only unique for the individual grippers belonging to a specific multi-gripper device.String getDisplayName()
The name of the gripper displayed in the PolyScope UI, e.g. in the Gripper toolbar and program node.
Note: This name must not be used to uniquely identify a specific individual gripper, since the name might be translated (depending on the selected language in PolyScope) or be changed between versions of the URCap that added the gripper.boolean isResolvable()
An individual gripper cannot be guaranteed to be present in PolyScope. This method can be used to determine, if the gripper is present.
The gripper will not be present if the owning multi-gripper device has disabled that specific individual gripper.true, if this individual gripper is present in PolyScope, otherwise false.Copyright © 2020. All rights reserved.