public interface WaypointBlendParameters extends BlendParameters
BlendParameters.ParameterType| Modifier and Type | Method and Description |
|---|---|
Blend |
getBlend()
Get the blend to be used for the movement.
|
getTypeBlend getBlend()
Get the blend to be used for the movement.
Note that, if the configuration has not been applied to a waypoint node in the program tree, the blend value returned is a "suggested" value, since the blend may be (automatically) corrected depending on surrounding waypoints in the program tree (when it is applied to a waypoint node).Copyright © 2020. All rights reserved.