public static enum VariablePositionWaypointNodeConfig.VariableDefinition extends Enum<VariablePositionWaypointNodeConfig.VariableDefinition>
| Enum Constant and Description |
|---|
DEFINED
A variable has been selected making this config defined.
|
UNDEFINED
A variable has not been selected.
|
| Modifier and Type | Method and Description |
|---|---|
static VariablePositionWaypointNodeConfig.VariableDefinition |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static VariablePositionWaypointNodeConfig.VariableDefinition[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final VariablePositionWaypointNodeConfig.VariableDefinition UNDEFINED
public static final VariablePositionWaypointNodeConfig.VariableDefinition DEFINED
A variable has been selected making this config defined.
Cast this instance toVariablePositionDefinedWaypointNodeConfig.public static VariablePositionWaypointNodeConfig.VariableDefinition[] values()
for (VariablePositionWaypointNodeConfig.VariableDefinition c : VariablePositionWaypointNodeConfig.VariableDefinition.values()) System.out.println(c);
public static VariablePositionWaypointNodeConfig.VariableDefinition valueOf(String name)
name - the name of the enum constant to be returned.IllegalArgumentException - if this enum type has no constant with the specified nameNullPointerException - if the argument is nullCopyright © 2020. All rights reserved.