| Interface | Description |
|---|---|
| DriveScrewNotOKParameters |
This interface provides parameters relevant for generating script code for the Drive Screw Not OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewNotOKCapability(ScriptCodeGenerator)). |
| DriveScrewOKParameters |
This interface provides parameters relevant for generating script code for the Drive Screw OK feedback capability
(registered using
ScrewdriverFeedbackCapabilities.registerDriveScrewOKCapability(ScriptCodeGenerator)). |
| FeedScrewParameters |
This interface provides parameters relevant for generating script code for the Feed Screw capability
(registered using
ScrewdriverCapabilities.registerFeedScrewCapability(ScriptCodeGenerator)). |
| PrepareToStartScrewdriverParameters |
This interface provides parameters relevant for generating script code for the Prepare To Start Screwdriver capability
(registered using
ScrewdriverCapabilities.registerPrepareToStartScrewdriverCapability(ScriptCodeGenerator)). |
| ProgramSelectionParameters |
This interface provides parameters relevant for generating script code for the Program Selection capability
(registered using
ScrewdriverCapabilities.registerProgramSelectionCapability(ScrewdriverProgramListProvider, ScriptCodeGenerator)). |
| ScrewdriverCapabilities |
Register the capabilities of the screwdriver using this interface.
|
| ScrewdriverFeedbackCapabilities |
Register the feedback capabilities of the screwdriver using this interface.
|
| ScrewdriverReadyParameters |
This interface provides the parameters relevant for generating script for the Screwdriver Ready feedback operation
capability (registered using
ScrewdriverFeedbackCapabilities.registerScrewdriverReadyCapability(ScriptCodeGenerator)). |
| Exception | Description |
|---|---|
| CapabilityAlreadyRegistered |
This exception is thrown when an attempt is made to register a capability that has already been registered.
|
Copyright © 2020. All rights reserved.