public interface JointPositions
This interface represents the positions of all of the joints in the robot arm.
AJointPositions object can be built using the JointPositionFactory interface.| Modifier and Type | Method and Description | 
|---|---|
boolean | 
epsilonEquals(JointPositions other,
             double epsilon,
             Angle.Unit unit)
Indicates whether each element of some other  
JointPositions object is "approximately equal" to this one. | 
boolean | 
equals(Object obj)
Indicates whether some other  
JointPositions object is "equal to" this one. | 
JointPosition[] | 
getAllJointPositions()
Provides the array of  
JointPosition values. | 
int | 
hashCode()  | 
String | 
toString()  | 
JointPosition[] getAllJointPositions()
JointPosition values.boolean epsilonEquals(JointPositions other, double epsilon, Angle.Unit unit)
JointPositions object is "approximately equal" to this one.other - another JointPositions object.epsilon - a tolerance in the specified unit type.unit - unit type of the epsilon tolerance.true if the value of this object is "approximately equal" to the value of the
 other argument; false otherwise.int hashCode()
boolean equals(Object obj)
JointPositions object is "equal to" this one.Copyright © 2020. All rights reserved.