public interface JointPositionFactory
| Modifier and Type | Method and Description | 
|---|---|
JointPositions | 
createJointPositions(double base,
                    double shoulder,
                    double elbow,
                    double wrist1,
                    double wrist2,
                    double wrist3,
                    Angle.Unit unit)
Creates a  
JointPositions object with six revolute joints using the provided angles and unit type. | 
JointPositions createJointPositions(double base, double shoulder, double elbow, double wrist1, double wrist2, double wrist3, Angle.Unit unit)
JointPositions object with six revolute joints using the provided angles and unit type.base - Base joint position.shoulder - Shoulder joint position.elbow - Elbow joint position.wrist1 - Wrist1 joint position.wrist2 - Wrist2 joint position.wrist3 - Wrist3 joint position.unit - the unit type for all the joint position arguments.JointPositions object.Copyright © 2020. All rights reserved.