| Interface | Description | 
|---|---|
| UserInteraction | 
 This interface provides functionality for requesting input or actions from end users 
 | 
| Class | Description | 
|---|---|
| RobotPositionCallback | Deprecated
 Use  
RobotPositionCallback2 instead. | 
| RobotPositionCallback2 | 
 The robot position callback based on  
PositionParameters which composes several parameters defining a position
 of the robot. | 
Copyright © 2020. All rights reserved.