public static enum AnalogInputModeConfig.ConfigType extends Enum<AnalogInputModeConfig.ConfigType>
Enum Constant and Description |
---|
ANALOG_INPUT_DOMAIN
The analog inputs in the connector in the robot tool are configured as standard general purpose analog
inputs.
|
TOOL_COMMUNICATION_INTERFACE
Both analog inputs in the connector in the robot tool are configured to be used as a Tool Communication
Interface (TCI).
|
Modifier and Type | Method and Description |
---|---|
static AnalogInputModeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AnalogInputModeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AnalogInputModeConfig.ConfigType ANALOG_INPUT_DOMAIN
The analog inputs in the connector in the robot tool are configured as standard general purpose analog inputs.
The config instance can be cast toAnalogInputDomainConfig
.public static final AnalogInputModeConfig.ConfigType TOOL_COMMUNICATION_INTERFACE
Both analog inputs in the connector in the robot tool are configured to be used as a Tool Communication
Interface (TCI). When this mode is enabled, all analog tool inputs are unavailable.
The config instance can be cast to CommunicationInterfaceConfig
.
public static AnalogInputModeConfig.ConfigType[] values()
for (AnalogInputModeConfig.ConfigType c : AnalogInputModeConfig.ConfigType.values()) System.out.println(c);
public static AnalogInputModeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2020. All rights reserved.