public interface AnalogInputDomainConfig extends AnalogInputModeConfig
This interface represents the analog input domain configuration for the two analog inputs in the Tool I/O Interface.
 To create a new configuration, see the AnalogInputModeConfigFactory interface which is accessible through
 ToolIOInterfaceControllable.getAnalogInputModeConfigFactory(). 
 To apply a configuration, see ToolIOInterfaceControllable.setAnalogInputModeConfig(AnalogInputModeConfig).
 
| Modifier and Type | Interface and Description | 
|---|---|
static class  | 
AnalogInputDomainConfig.AnalogDomain
The type of the electrical domain used by the analog inputs in the connector in the robot tool 
 | 
AnalogInputModeConfig.ConfigType| Modifier and Type | Method and Description | 
|---|---|
AnalogInputDomainConfig.AnalogDomain | 
getAnalogDomainForInput0()
This method returns the type of electrical domain used by analog input 0 in the connector in the robot tool
 (labeled 'analog_in[2]' in PolyScope) 
 | 
AnalogInputDomainConfig.AnalogDomain | 
getAnalogDomainForInput1()
This method returns the type of electrical domain used by analog input 1 in the connector in the robot tool
 (labeled 'analog_in[3]' in PolyScope). 
 | 
getConfigTypeAnalogInputDomainConfig.AnalogDomain getAnalogDomainForInput0()
AnalogInputDomainConfig.AnalogDomain getAnalogDomainForInput1()
Copyright © 2020. All rights reserved.