| Interface | Description | 
|---|---|
| ContributionProvider<C> | 
 This interfaces provides access to a contribution. 
 | 
| DaemonContribution | 
 
 Defines an API definition that gives control of a daemon that belongs to a URCap. 
 | 
| DaemonService | 
 Defines an API that makes it possible to define daemons of a URCap within PolyScope. 
 | 
| InstallationNodeContribution | 
 API for installation node contributions. 
 | 
| InstallationNodeService | 
 Defines an API required for definition of an installation node and screen of a URCap. 
 | 
| NonUserInsertable | 
 
 This interface is a marker interface that can be used in combination with  
ProgramNodeService. | 
| ProgramNodeConfiguration | 
 Provides access to configure additional properties of a program node contribution with a HTML-based user interface. 
 | 
| ProgramNodeContribution | 
 Defines an API required for specifying a URCap Program Node within PolyScope. 
 | 
| ProgramNodeService | 
 Defines an API required for adding a new type of program node to PolyScope. 
 | 
| ProgramNodeServiceConfigurable | 
 This interface can be used in combination with the  
ProgramNodeService interface. | 
| URCapProgramNodeService | |
| ViewAPIProvider | 
 
 Provides access to functionality relevant for the View (UI) of an installation or a program node
 contribution. 
 | 
| Enum | Description | 
|---|---|
| DaemonContribution.State | 
 The run state of the daemon 
 | 
Copyright © 2020. All rights reserved.