public interface DaemonService
| Modifier and Type | Method and Description | 
|---|---|
URL | 
getExecutable()
Implement this method so that it returns an URL to the daemon executable resource inside the jar
 that contains the implementation of DaemonService. 
 | 
void | 
init(DaemonContribution daemon)
This method is called from PolyScope when the daemon service is registered by
 PolyScope. 
 | 
void init(DaemonContribution daemon)
DaemonContribution object control is set by PolyScope. The object can be used to install,
 start, stop, and monitor the registered daemon.daemon - - object that is used to install, control, and monitor the registered daemon.URL getExecutable()
Copyright © 2020. All rights reserved.