| Class and Description |
|---|
| WaitNodeConfig |
| WaitNodeConfigFactory
The WaitNodeConfigFactory can be used to construct configurations that can be set on a WaitNode.
|
| Class and Description |
|---|
| AnalogInputCurrentWaitNodeConfig |
| AnalogInputSelection |
| AnalogInputSelection.SelectionType |
| AnalogInputVoltageWaitNodeConfig |
| AnalogInputWaitNodeConfig |
| DigitalInputSelection |
| DigitalInputSelection.SelectionType |
| DigitalInputWaitNodeConfig |
| ExpressionInputWaitNodeConfig |
| FloatRegisterInputSelection |
| FloatRegisterInputSelection.SelectionType |
| FloatRegisterInputWaitNodeConfig |
| TimeWaitNodeConfig |
| WaitNodeConfig |
| WaitNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2019. All rights reserved.