public interface PoseFactory
This interface provides methods for creating poses in Cartesian space (relative to a reference coordinate system).
A pose can, e.g. describe the position of the robot tool (e.g. w.r.t. to robot base) or the TCP offset (relative to the center of the tool output flange).Modifier and Type | Method and Description |
---|---|
Pose |
createPose(double x,
double y,
double z,
double rx,
double ry,
double rz,
Length.Unit lengthUnit,
Angle.Unit angleUnit)
Creates a
Pose object with the specified Cartesian position and orientation (rotation). |
Pose createPose(double x, double y, double z, double rx, double ry, double rz, Length.Unit lengthUnit, Angle.Unit angleUnit)
Pose
object with the specified Cartesian position and orientation (rotation).x
- X coordinate of the position.y
- Y coordinate of the position.z
- Z coordinate of the position.rx
- Rx parameter of the rotation vector specifying the orientation.ry
- Ry parameter of the rotation vector specifying the orientation.rz
- Rz parameter of the rotation vector specifying the orientation.lengthUnit
- type of unit for the position.angleUnit
- type of unit for the rotation.Copyright © 2019. All rights reserved.