public interface CapabilityManager
This interface can be used to query whether or not a specific capability is available on the underlying robot/system.
A capability is a feature which may or may not be present on a given robot/system. The feature can be hardware-based or software-based (e.g. certain types of program nodes). Some hardware capabilities are not available on all robot platforms, e.g. the Tool Communication Interface functionality is not present on CB3 robots.
Modifier and Type | Method and Description |
---|---|
boolean |
hasCapability(Capability capability)
Verify availability of a capability on the robot/system.
|
boolean hasCapability(Capability capability)
capability
- to verify the presence of.true
if the capability is available.Copyright © 2019. All rights reserved.