Package | Description |
---|---|
com.ur.urcap.api.domain.resource | |
com.ur.urcap.api.domain.resource.tooliointerface.control |
Class and Description |
---|
ToolIOInterfaceController
This interface can be implemented to request control of the Tool I/O Interface.
|
Class and Description |
---|
AnalogInputModeConfigFactory
Factory for creating configurations of the analog input mode for the analog inputs in the connector in the robot tool.
|
DigitalOutputModeConfigFactory
Factory for creating configurations of the digital output mode for the digital outputs in the connector in the robot
tool.
|
ToolIOInterfaceControlEvent
This interface holds information relevant to the
ToolIOInterfaceController.onControlGranted(ToolIOInterfaceControlEvent)
and ToolIOInterfaceController.onControlToBeRevoked(ToolIOInterfaceControlEvent) events that occur when
the control of the Tool I/O Interface resource has been assigned to a URCap or when the control is about to be revoked,
respectively. |
ToolIOInterfaceControllable
This is an interface for controlling/configuring the settings of the Tool I/O Interface
|
Copyright © 2019. All rights reserved.