Package | Description |
---|---|
com.ur.urcap.api.domain.resource.tooliointerface | |
com.ur.urcap.api.domain.resource.tooliointerface.control |
Modifier and Type | Method and Description |
---|---|
StandardDigitalOutputModeConfig.OutputMode |
StandardDigitalOutputModeConfig.getOutputModeForOutput0() |
StandardDigitalOutputModeConfig.OutputMode |
StandardDigitalOutputModeConfig.getOutputModeForOutput1() |
static StandardDigitalOutputModeConfig.OutputMode |
StandardDigitalOutputModeConfig.OutputMode.valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static StandardDigitalOutputModeConfig.OutputMode[] |
StandardDigitalOutputModeConfig.OutputMode.values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
Modifier and Type | Method and Description |
---|---|
StandardDigitalOutputModeConfig |
DigitalOutputModeConfigFactory.createStandardDigitalOutputModeConfig(StandardDigitalOutputModeConfig.OutputMode output0,
StandardDigitalOutputModeConfig.OutputMode output1)
Create a configuration to set the digital output mode for each of the digital outputs in the connector in the
robot tool.
|
Copyright © 2019. All rights reserved.