public static enum WaypointNodeConfig.ConfigType extends Enum<WaypointNodeConfig.ConfigType>
Enum Constant and Description |
---|
FIXED_POSITION
Fixed position has been selected (fixed waypoint).
|
RELATIVE_POSITION
Relative position has been selected (relative waypoint).
|
VARIABLE_POSITION
Variable position has been selected (variable waypoint).
|
Modifier and Type | Method and Description |
---|---|
static WaypointNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static WaypointNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final WaypointNodeConfig.ConfigType FIXED_POSITION
Fixed position has been selected (fixed waypoint).
The config instance can be cast toFixedPositionWaypointNodeConfig
.public static final WaypointNodeConfig.ConfigType RELATIVE_POSITION
public static final WaypointNodeConfig.ConfigType VARIABLE_POSITION
Variable position has been selected (variable waypoint).
The config instance can be cast toVariablePositionWaypointNodeConfig
.public static WaypointNodeConfig.ConfigType[] values()
for (WaypointNodeConfig.ConfigType c : WaypointNodeConfig.ConfigType.values()) System.out.println(c);
public static WaypointNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.