public static enum WaypointMotionParameters.ParameterType extends Enum<WaypointMotionParameters.ParameterType>
Enum Constant and Description |
---|
JOINT_MOTION
Joint motion parameters has been selected.
|
SHARED_MOTION
Shared motion parameters has been selected.
|
TIME_MOTION
Time motion parameters has been selected.
|
TOOL_MOTION
Tool motion parameters has been selected.
|
Modifier and Type | Method and Description |
---|---|
static WaypointMotionParameters.ParameterType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static WaypointMotionParameters.ParameterType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final WaypointMotionParameters.ParameterType TIME_MOTION
Time motion parameters has been selected.
This instance can be cast toTimeMotionParameters
.public static final WaypointMotionParameters.ParameterType JOINT_MOTION
Joint motion parameters has been selected.
This instance can be cast toJointMotionParameters
.public static final WaypointMotionParameters.ParameterType TOOL_MOTION
Tool motion parameters has been selected.
This instance can be cast toToolMotionParameters
.public static final WaypointMotionParameters.ParameterType SHARED_MOTION
public static WaypointMotionParameters.ParameterType[] values()
for (WaypointMotionParameters.ParameterType c : WaypointMotionParameters.ParameterType.values()) System.out.println(c);
public static WaypointMotionParameters.ParameterType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.