public static enum CustomDecelerationParameters.Type extends Enum<CustomDecelerationParameters.Type>
Enum Constant and Description |
---|
Angular
This deceleration is currently used under a MoveJ node.
|
Cartesian
This deceleration is currently used under a MoveL or MoveP node.
|
Unknown
This deceleration was either created specifying values for both
AngularAcceleration and Acceleration
and/or is in use in an Until node that is not yet in the program tree. |
Modifier and Type | Method and Description |
---|---|
static CustomDecelerationParameters.Type |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static CustomDecelerationParameters.Type[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final CustomDecelerationParameters.Type Unknown
AngularAcceleration
and Acceleration
and/or is in use in an Until node that is not yet in the program tree.public static final CustomDecelerationParameters.Type Angular
public static final CustomDecelerationParameters.Type Cartesian
public static CustomDecelerationParameters.Type[] values()
for (CustomDecelerationParameters.Type c : CustomDecelerationParameters.Type.values()) System.out.println(c);
public static CustomDecelerationParameters.Type valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.