public static enum SetNodeConfig.ConfigType extends Enum<SetNodeConfig.ConfigType>
Enum Constant and Description |
---|
ANALOG_OUTPUT_CURRENT
Analog output configured for electric current or no output has been selected.
|
ANALOG_OUTPUT_VOLTAGE
Analog output configured for voltage has been selected.
|
DIGITAL_OUTPUT
Digital output has been selected.
|
EXPRESSION_OUTPUT
Expression output has been selected.
|
FLOAT_REGISTER_OUTPUT
Register using float type values has been selected.
|
INCREMENT_VARIABLE
Increment variable has been selected.
|
NO_ACTION
No action has been selected.
|
NO_TYPE
No selection has been made.
|
SINGLE_DIGITAL_PULSE
Single digital pulse output has been selected.
|
Modifier and Type | Method and Description |
---|---|
static SetNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static SetNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final SetNodeConfig.ConfigType NO_TYPE
public static final SetNodeConfig.ConfigType NO_ACTION
public static final SetNodeConfig.ConfigType DIGITAL_OUTPUT
Digital output has been selected.
The config instance can be cast toDigitalOutputSetNodeConfig
.public static final SetNodeConfig.ConfigType ANALOG_OUTPUT_CURRENT
Analog output configured for electric current or no output has been selected.
The config instance can be cast toAnalogOutputCurrentSetNodeConfig
.public static final SetNodeConfig.ConfigType ANALOG_OUTPUT_VOLTAGE
Analog output configured for voltage has been selected.
The config instance can be cast toAnalogOutputVoltageSetNodeConfig
.public static final SetNodeConfig.ConfigType FLOAT_REGISTER_OUTPUT
Register using float type values has been selected.
The config instance can be cast toFloatRegisterOutputSetNodeConfig
.public static final SetNodeConfig.ConfigType EXPRESSION_OUTPUT
Expression output has been selected.
The config instance can be cast toExpressionOutputSetNodeConfig
.public static final SetNodeConfig.ConfigType SINGLE_DIGITAL_PULSE
Single digital pulse output has been selected.
The config instance can be cast toSingleDigitalPulseSetNodeConfig
.public static final SetNodeConfig.ConfigType INCREMENT_VARIABLE
Increment variable has been selected. This type has no further information.
Setting this type of config will be ignored and will have no effect on the node.public static SetNodeConfig.ConfigType[] values()
for (SetNodeConfig.ConfigType c : SetNodeConfig.ConfigType.values()) System.out.println(c);
public static SetNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.