public static enum ForceNodeConfig.ConfigType extends Enum<ForceNodeConfig.ConfigType>
Enum Constant and Description |
---|
FRAME
Frame type is selected.
|
MOTION
Motion type is selected.
|
POINT
Point type is selected.
|
SIMPLE
Simple type is selected.
|
Modifier and Type | Method and Description |
---|---|
static ForceNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static ForceNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final ForceNodeConfig.ConfigType SIMPLE
Simple type is selected. This type has no further information.
Setting this type of config will be ignored and will have no effect on the node.public static final ForceNodeConfig.ConfigType FRAME
Frame type is selected.
The config instance can be cast toFrameForceNodeConfig
.public static final ForceNodeConfig.ConfigType POINT
Point type is selected. This type has no further information.
Setting this type of config will be ignored and will have no effect on the node.public static final ForceNodeConfig.ConfigType MOTION
Motion type is selected. This type has no further information.
Setting this type of config will be ignored and will have no effect on the node.public static ForceNodeConfig.ConfigType[] values()
for (ForceNodeConfig.ConfigType c : ForceNodeConfig.ConfigType.values()) System.out.println(c);
public static ForceNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.