public static enum DirectionSelection.SelectionType extends Enum<DirectionSelection.SelectionType>
Enum Constant and Description |
---|
AXIS
Direction is specified using an Axis.
|
EXPRESSION
A direction vector is specified using an Expression.
|
Modifier and Type | Method and Description |
---|---|
static DirectionSelection.SelectionType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static DirectionSelection.SelectionType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final DirectionSelection.SelectionType EXPRESSION
A direction vector is specified using an Expression.
The Selection instance can be cast toDirectionVectorExpression
.public static final DirectionSelection.SelectionType AXIS
Direction is specified using an Axis.
The Selection instance can be cast toDirectionAxis
.public static DirectionSelection.SelectionType[] values()
for (DirectionSelection.SelectionType c : DirectionSelection.SelectionType.values()) System.out.println(c);
public static DirectionSelection.SelectionType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.