public interface PopupNode extends ProgramNode
Modifier and Type | Interface and Description |
---|---|
static class |
PopupNode.Type |
Modifier and Type | Method and Description |
---|---|
String |
getMessage() |
PopupNode.Type |
getType() |
PopupNode |
setMessage(String message) |
PopupNode |
setType(PopupNode.Type type) |
PopupNode setMessage(String message)
message
- the message in the pop up for the end userIllegalStateException
- if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager
)String getMessage()
PopupNode setType(PopupNode.Type type)
type
- the type of pop upIllegalStateException
- if called from a Swing-based URCap outside of an UndoableChanges
scope (see also UndoRedoManager
)PopupNode.Type getType()
Copyright © 2019. All rights reserved.