IO.InterfaceType, IO.IOType
Modifier and Type | Method and Description |
---|---|
double |
getMaxRangeValue() |
double |
getMinRangeValue() |
double |
getValue() |
boolean |
isCurrent() |
boolean |
isResolvable()
Some analog I/Os, such as the analog tool inputs, are in some situations not available for use.
|
boolean |
isVoltage() |
boolean |
setValue(double value)
Set analog I/O output signal.
|
getDefaultName, getInterfaceType, getName, getType, getValueStr, isInput
double getMinRangeValue()
double getMaxRangeValue()
boolean isCurrent()
boolean isVoltage()
boolean setValue(double value)
value
- The analog value to be set.true
if the analog signal was set, false
if the signal was not set, e.g. because the
controller was not running.double getValue()
boolean isResolvable()
isResolvable
in interface IO
true
, if the analog signal is available.
false
otherwise, e.g. because an analog tool input is used for Tool Communication Interface (TCI).Copyright © 2019. All rights reserved.