Interface | Description |
---|---|
CustomUserInputConfiguration |
This interface handles registration of custom user inputs (typically for device configuration in an installation node).
|
TextComponent |
This interface represents a text UI element for displaying information to the end user.
|
UserInput<T> |
A generic interface which provides access to the value entered or selected by the end user.
|
ValueChangedListener<T> |
This interface can be used to listen for changes of the value of a user input.
|
Exception | Description |
---|---|
CalledOutsideUserInputConfigurationPhase |
This exception is thrown when calls to any of the methods in the
CustomUserInputConfiguration interface (e.g. |
CannotAccessDeprecatedUserInput |
This exception is thrown when an attempt is made to access a user input, e.g.
|
IDAlreadyDefined |
This exception is thrown when an attempt is made to register a new user input with an identifier which has already
been used to register a different user input.
|
TooManyUserInputsRegistered |
This exception is thrown if the maximum allowed number of registered user inputs will be exceeded when attempting to
register a new user input.
|
Copyright © 2019. All rights reserved.