Modifier and Type | Method and Description |
---|---|
void |
setErrorValidator(InputValidator<Double> validator)
Set a custom input validator for detecting errors for the user input.
|
getValue, setValueChangedListener
void setErrorValidator(InputValidator<Double> validator)
Set a custom input validator for detecting errors for the user input.
Note: By default, a range validator verifying that the input value is between the specified minimum and maximum value is always attached to the user input.validator
- the custom error input validatorCopyright © 2019. All rights reserved.