public abstract class RobotMovementCallback extends Object
| Constructor and Description | 
|---|
RobotMovementCallback()  | 
| Modifier and Type | Method and Description | 
|---|---|
void | 
onCancel(MovementCancelEvent event)
This method is called if the user cancels the move request (before reaching the target position). 
Overriding this method is optional.  | 
abstract void | 
onComplete(MovementCompleteEvent event)
This method is called when the robot has been moved to the desired target position by the user. 
This method must be overridden.  | 
void | 
onError(MovementErrorEvent event)
This method is called when an error occurs in the move request. 
 | 
public abstract void onComplete(MovementCompleteEvent event)
event - This object holds information related to the onComplete event.public void onCancel(MovementCancelEvent event)
event - This object holds information related to the onCancel event.public void onError(MovementErrorEvent event)
event - This object holds information related to the onError event.Copyright © 2019. All rights reserved.