public interface WaitNode extends ProgramNode
| Modifier and Type | Method and Description | 
|---|---|
WaitNodeConfig | 
getConfig()  | 
WaitNodeConfigFactory | 
getConfigFactory()  | 
WaitNode | 
setConfig(WaitNodeConfig config)
Set a configuration on this node. 
 | 
WaitNodeConfigFactory getConfigFactory()
WaitNode setConfig(WaitNodeConfig config)
config - the configuration to be set.InvalidDomainException - if config is analog input using voltage and the IO is configured to current
 or vice versa.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)WaitNodeConfig getConfig()
Copyright © 2019. All rights reserved.