| Class and Description | 
|---|
| WaitNodeConfig | 
| WaitNodeConfigFactory
 The WaitNodeConfigFactory can be used to construct configurations that can be set on a WaitNode. 
 | 
| Class and Description | 
|---|
| AnalogInputCurrentWaitNodeConfig | 
| AnalogInputSelection | 
| AnalogInputSelection.SelectionType | 
| AnalogInputVoltageWaitNodeConfig | 
| AnalogInputWaitNodeConfig | 
| DigitalInputSelection | 
| DigitalInputSelection.SelectionType | 
| DigitalInputWaitNodeConfig | 
| ExpressionInputWaitNodeConfig | 
| FloatRegisterInputSelection | 
| FloatRegisterInputSelection.SelectionType | 
| FloatRegisterInputWaitNodeConfig | 
| TimeWaitNodeConfig | 
| WaitNodeConfig | 
| WaitNodeConfig.ConfigType
 The configuration type used to determine which type of configuration this instance is. 
 | 
Copyright © 2019. All rights reserved.