public static enum DecelerationParameters.ParameterType extends Enum<DecelerationParameters.ParameterType>
Enum Constant and Description |
---|
CUSTOM_DECELERATION
Custom deceleration has been selected.
|
SHARED_DECELERATION
Shared deceleration has been selected.
|
Modifier and Type | Method and Description |
---|---|
static DecelerationParameters.ParameterType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static DecelerationParameters.ParameterType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final DecelerationParameters.ParameterType SHARED_DECELERATION
public static final DecelerationParameters.ParameterType CUSTOM_DECELERATION
CustomDecelerationParameters
public static DecelerationParameters.ParameterType[] values()
for (DecelerationParameters.ParameterType c : DecelerationParameters.ParameterType.values()) System.out.println(c);
public static DecelerationParameters.ParameterType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2019. All rights reserved.