| Class and Description | 
|---|
| AssignmentNodeConfig | 
| AssignmentNodeConfigFactory
 The AssignmentNodeConfigFactory can be used to construct configurations that can be set on a AssignmentNode. 
 | 
| Class and Description | 
|---|
| AssignmentNodeConfig | 
| AssignmentNodeConfig.ConfigType
 The configuration type used to determine which type of configuration this instance is. 
 | 
| ExpressionAssignmentNodeConfig | 
Copyright © 2019. All rights reserved.