public interface TCPContributionModel
Note: This interface must only be used in an installation contribution.
| Modifier and Type | Method and Description |
|---|---|
TCP |
addTCP(String idKey,
String suggestedName,
Pose offset)
Add a TCP to the current PolyScope installation.
|
TCP |
getTCP(String idKey)
Returns the TCP previously added by this URCap using the same
idKey. |
void |
removeTCP(String idKey)
Remove a TCP added by this URCap from PolyScope.
|
void |
updateTCP(String idKey,
Pose newOffset)
Update the offset of a TCP already added by this URCap.
|
TCP addTCP(String idKey, String suggestedName, Pose offset)
idKey - The key to identify this TCP by. The key is for this URCap only, i.e. it only has to be unique for this
URCap and not "globally" for other URCaps.suggestedName - Suggested name for the TCP. Valid names must match regex [a-zA-Z][a-zA-Z0-9_]{0,14} for a total
of 15 characters. The final name can be retrieved from the returned TCP instance.offset - The offset of the TCP with respect to the tool output flangeTCPAlreadyAddedException - If called twice using the same idKey.
Use getTCP(String) to check if the TCP has already been added to the current installation.
Use updateTCP(String, Pose) to update the TCP if the offset of the TCP has changed.IllegalTCPNameException - If the suggested name does not match required regex.IllegalArgumentException - If the pose specified for the offset is not inside the valid range of a TCP offset as
defined by PolyScope.TCP getTCP(String idKey)
idKey. Use this to verify if the TCP is
present in the current installation.idKey - The key to identify this TCP by.void updateTCP(String idKey, Pose newOffset)
idKey - The key to identify the TCP. A TCP must have been added prior to this method call using the same key.newOffset - The new offset to set for the TCP with respect to the tool output flangeTCPNotFoundException - If no TCP exists with the provided idKey.IllegalArgumentException - If the pose specified for the offset is not inside the valid range of a TCP offset as
defined by PolyScope.void removeTCP(String idKey)
idKey - The key used to add the TCP with.TCPNotFoundException - If no TCP exists with the provided idKey.Copyright © 2018. All rights reserved.