public interface TreeNode
ProgramModel.getRootTreeNode(ProgramNodeContribution) to obtain a root for the sub-tree, it is possible to add children.
For each call to addChild(ProgramNode), a new TreeNode is returned, that can, in turn, act as a root for yet another sub-tree.| Modifier and Type | Method and Description |
|---|---|
TreeNode |
addChild(ProgramNode programNode)
Add a child to this TreeNode
|
List<TreeNode> |
getChildren() |
ProgramNode |
getProgramNode() |
TreeNode |
insertChildAfter(TreeNode existingChildNode,
ProgramNode programNode)
Inserts a child under this TreeNode directly after the existing selected child node.
|
TreeNode |
insertChildBefore(TreeNode existingChildNode,
ProgramNode programNode)
Inserts a child under this TreeNode directly before the existing selected child node.
|
boolean |
removeChild(TreeNode child)
Removes a child from the sub-tree.
|
TreeNode |
setChildSequenceLocked(boolean isChildSequenceLocked)
Means that the children can not be rearranged, deleted or have other nodes inserted into the child sequence by the end user.
|
void |
traverse(ProgramNodeVisitor nodeVisitor)
This method traverses the entire sub-tree under this tree node in a depth-first fashion (this corresponds to a
top-down approach in the program tree).
|
TreeNode addChild(ProgramNode programNode) throws TreeStructureException
programNode - the ProgramNode constructed using the ProgramNodeFactoryTreeStructureException - If it is not allowed to insert the ProgramNode at this position a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)TreeNode insertChildBefore(TreeNode existingChildNode, ProgramNode programNode) throws TreeStructureException
existingChildNode - existing TreeNode child of this TreeNodeprogramNode - the ProgramNode constructed using the ProgramNodeFactoryTreeStructureException - If it is not allowed to insert the ProgramNode at this position or if the selected child node is not a child of this TreeNode a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)TreeNode insertChildAfter(TreeNode existingChildNode, ProgramNode programNode) throws TreeStructureException
existingChildNode - existing TreeNode child of this TreeNodeprogramNode - the ProgramNode constructed using the ProgramNodeFactoryTreeStructureException - If it is not allowed to insert the ProgramNode at this position or if the selected child node is not a child of this TreeNode a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)boolean removeChild(TreeNode child) throws TreeStructureException
child - The TreeNode child to be removed.TreeStructureException - If the removed child would leave the tree in an illegal state a TreeStructureException will be thrown.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)List<TreeNode> getChildren()
ProgramNode getProgramNode()
ProgramNode at this position in the sub-tree.
Can either be a built-in PolyScope program node (provided by Universal Robots) or a URCap program node.TreeNode setChildSequenceLocked(boolean isChildSequenceLocked)
isChildSequenceLocked - If true then the immediate children under this TreeNode will be lockedvoid traverse(ProgramNodeVisitor nodeVisitor)
ProgramNodeVisitor implementation with optional overrides or
a URCapProgramNodeInterfaceVisitor implementation. In the latter
case, the URCapProgramNodeInterfaceVisitor.visitURCapAs(Object, int, int) method must be implemented.
The URCapProgramNodeInterfaceVisitor can be used when targeting URCap program nodes implementing the (generic) type parameter
specified in URCapProgramNodeInterfaceVisitor (see also URCapProgramNode.getAs(Class)).
Note that this method is sometimes called accept() in the Visitor software design pattern.nodeVisitor - the instance callbacks are made to.Copyright © 2018. All rights reserved.