public static enum AssignmentNodeConfig.ConfigType extends Enum<AssignmentNodeConfig.ConfigType>
Enum Constant and Description |
---|
EXPRESSION
Expression assignment has been selected.
|
OPERATOR
Operator assignment has been selected.
|
Modifier and Type | Method and Description |
---|---|
static AssignmentNodeConfig.ConfigType |
valueOf(String name)
Returns the enum constant of this type with the specified name.
|
static AssignmentNodeConfig.ConfigType[] |
values()
Returns an array containing the constants of this enum type, in
the order they are declared.
|
public static final AssignmentNodeConfig.ConfigType EXPRESSION
ExpressionAssignmentNodeConfig
public static final AssignmentNodeConfig.ConfigType OPERATOR
public static AssignmentNodeConfig.ConfigType[] values()
for (AssignmentNodeConfig.ConfigType c : AssignmentNodeConfig.ConfigType.values()) System.out.println(c);
public static AssignmentNodeConfig.ConfigType valueOf(String name)
name
- the name of the enum constant to be returned.IllegalArgumentException
- if this enum type has no constant with the specified nameNullPointerException
- if the argument is nullCopyright © 2018. All rights reserved.